4/18/2019 1:53 PM | |
Joined: 1/4/2007 Last visit: 4/18/2024 Posts: 1111 Rating: (174)
|
Hello Urantia, Thank you very much for your Siwatool-file. Well, into your Siwatool-file, I can see into the error message buffer, that there is often the error message: It seems, as if the FTA rejects often your commands !?! I checked your parameter settings, but I saw no issues! Also I downloaded your Siwatool-file to my Siwarex FTA, and it was possible for me to start a dosing. Therefore I have a wish to you: (I’m interested in that new Siwatool-file: Best regards Siwarexi Attachmentcreate_a_SIWATOOL_V2-file.pdf (189 Downloads) |
5/8/2019 11:37 PM | |
Joined: 10/23/2009 Last visit: 3/11/2024 Posts: 114 Rating: (0) |
Dear Siwarexi, Sorry for my late answer. Please find attached the file. In this case the error was the PLC did not recieve the STA_DOSING_STEP_2. Change .txt by .fta Thanks in advance. AttachmentOil Scale 20190508_1306.txt (206 Downloads) |
5/10/2019 1:33 PM | |
Joined: 1/4/2007 Last visit: 4/18/2024 Posts: 1111 Rating: (174)
|
Hello Urantia, Thanks for your Siwatool file. I guess, I found your issue! Into your Siwatool file, I can see that you had the error message: „Data Data- / operating-error 141: Start not possible since set value > max. permitted set value That means: The Start is not possible because the defined set value does not match the current scale status. The following must apply: Current gross + set value (DR20) – current trailing + shut-off correction value < maximum weighing range Into your Siwatool file the parameters are: - Gross process value (DR30): -0.053 kg - Set weight (DR20): 61.861 kg - Trailing weight (DR22): 1.0 kg - Shut-off correction value (DR22): 0.0 kg - Maximum weight for weighing range 1 (DR3): 60.0 kg The calculation is: -0.053 kg + 61.861 kg – 1.0 kg + 0.0 kg < 60.0 kg 60.808 < 60.0 <= THAT’S WRONG! Or in shorter words: Your set weight (= 61.861 kg) is larger than the defined weighing range in the DR3 (= 60 kg). One question: Can you increase the weighing range in DR3? Best regards Siwarexi |
Follow us on