Industry Online Support
Technical Forum
11/14/2007 11:17 AM | |
Posts: 2930 Rating: (432) |
Hi Guillaume, What is the S7-200 Explorer verison and what Execl Version do you use? I had a similar problem in the past with Office 2000 and an older S7-200 Explorer version. Can you post your datalog record so I can have a look if Office 2003 works. I think the problem was fixed on my PC by updating MS Office from 2000 to 2003. Regards Helmut |
11/14/2007 1:56 PM | |
Posts: 3 Rating: (0) |
my s7-200 network version 5 internet exploren version 6 I think it is an new problem. Watch the data at the attachement. The first row is an correct one but the values are with semicolon separated. The second row: The date and time colom are well separated but the next colom....... S7-200 add .0 (dot zero) to the value. Watch the both last coloms they are spare. The actual VD variable is zero. Once I start calculating... first AIW to double integer then double integer to real then divided with 10.0.... Thanks in advance Wim AttachmentThermoLogFile - 14-11-2007 9-06.zip (130 Downloads) |
11/14/2007 2:03 PM | |
Posts: 3 Rating: (0) |
I used for the first colom VD900 second VD904 908 912 916 920. With the wizard I choose VB900 as offset. Then placed 6 fields with the 'real' label and the wizard generates the correct amount of space VB900 VB923. |
Last edited by: Guillaume at: 14.11.2007 14:04 |
|
Follow us on