10/21/2015 9:54 AM | |
Posts: 38 Rating: (0) |
Hello For my project it is necessary to read one line at a time in a CSV file. I have used the siemens example used here: Tutorial I can see only one line of the file, but I need to see one line, and when I press next it needs to show me the next line of the file. Is it possible to do this in the scripting? I've attached an example of my file. |
10/21/2015 2:04 PM | |
Posts: 8946 Rating: (999) |
Perhaps this link may help you. It is for WinCCflexible, but it is helpfully also for TIA: |
This contribution was helpful to1 thankful Users |
Follow us on