1/2/2014 7:54 AM | |
Posts: 16 Rating: (0) |
Good day I have downloaded a example program for text file reading and writing in WinCC flexible SP3 from the following link. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=26106418&caller=SR&caller=view I was able to read and write in the .text and .csv file, but when i open the script an error comes and the program shuts down the error message file is attached herewith, can anybody help me in resolving this problem. Thanks Viquar Attachmenterror image.zip (87 Downloads) |
1/2/2014 8:24 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147)
|
Hello, Are you using the latest updates for WinCC flexible 2008 SP3? Here you can download: Update for WinCC flexible 2008 Service Pack 3 Best regards, Wizard |
1/2/2014 8:28 AM | |
Posts: 16 Rating: (0) |
Thanks for the reply I am using WinCC flexible SP3 only, however I download and check from the link also. |
1/2/2014 10:27 AM | |
Posts: 16 Rating: (0) |
Hi I have downloaded the updated4 for WinCC flexible and installed, still the same problem, scrip doesn't open. Best regards Farooq
|
1/2/2014 11:04 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147)
|
Hi, I downloaded the sample program. I have also WinCC flexible 2008 SP3 + Upd4 and can open the script without problems. Perhaps you can try the following: Go to Options -> Delete temporary files And then compile the project again. Or reset WinCC flexible: how can you reset WinCC flexible to the original status of the last installation? Best regards, Wizard |
This contribution was helpful to2 thankful Users |
1/2/2014 12:49 PM | |
Posts: 16 Rating: (0) |
Dear Sir Thanks for the support. I have done both the things but it's not working, please have a look at the attached error file, you may get exact information. Regards Farooq Attachmenterror report.zip (53 Downloads) |
1/2/2014 1:11 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147)
|
Hi I'm sorry but I have no idea. I think it is better to start a Support Request Let us know the result. Best regards, Wizard |
1/2/2014 1:47 PM | |
Posts: 16 Rating: (0) |
Hi I will do so and will let you know the result Thanks....... |
1/3/2014 7:57 AM | |
Posts: 16 Rating: (0) |
Dear Sir PLease find the attached scrip. Best Regards Farooq AttachmentRead_data_from_a_file_PC.pdf (461 Downloads) |
Follow us on