8/30/2014 8:29 AM | |
Posts: 5225 Rating: (1187) |
Do you know how I can in WinCC TIA convert 2 integer to 1 double integer ? Hi there. Could you explain please why you want to do this? In other words what type of combination would you want to make? Do you have access to the source of the two INT values? w |
9/1/2014 8:00 AM | |
Posts: 21 Rating: (0) |
Hello William, Thanks for your reaction. In fact an external device is delivering a 32 bits value. TIA WinCC Advanced can read the value in the OPC Server from this external device on the same PC. I do not have access to the source and the external device it is not a PLC. But each value is given as 2 successive 16 bits words in the OPC Server. When the value is smaller than 65535 then it is OK but when higher than I need to compose these 2 words values. So I need a kind of “Make Double Word” function. Best regards |
Follow us on