3/23/2011 7:12 AM | |
Joined: 12/2/2010 Last visit: 4/2/2024 Posts: 61 Rating: (0) |
Dear Experts is it possible to convert a REALinto DWORD? |
Regards \ Sankar |
|
3/23/2011 7:40 AM | |
Joined: 12/2/2010 Last visit: 4/2/2024 Posts: 61 Rating: (0) |
Thanks... |
Regards \ Sankar |
|
3/23/2011 9:40 PM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359) |
Also check this :
CPU can interpret 32- bit memory area as a real number or a double word(digital number with structure explained above). this depends on the codes used to handle the variable. case1: [code] L MD 0 L 3.141500e+000 *R //MD0 is considered a real number T MD 4 [/code] case2: [code] L MD 0 //MD0 is considered a Double word digital value L DW#16#A0A0 AD T MD 4[/code] BR |
Last edited by: hdhosseini at: 3/23/2011 9:42 PM |
|
Follow us on