7/8/2013 8:33 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Third? ! |
7/8/2013 3:56 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477) |
Its already… in campaign time, this kinds of threads got most no of views and replies
100 % Agree... As Moderators says- this is to boost activity here and I think they are being succeeded Also agree with AMAZINGAHMED that during some times, few regular members are also being inactive and campaign force them to be here and be active So many new member joins campaign and they may attract to come here often because they get their solutions very fast during this time. I said earlier too that I also joined forum to get help to solve one of my problem and at that time I got very quick replies which impressed me a lot and that’s why I am here from then I agree that some times campaign becomes annoying when some people just give reply with change in phrase of previous reply. We can not change these things so my thinking is, just ignore that Here one more thing I observed is criticizing this campaign – so many users are discussing so many bad things about campaign – even some of them are doing bad but discussing here also – These all should be stopped. All issues and feedback and all related to campaign should be shared only after campaign finish (or even after premium distributed) – that will make healthy discussion amongst the regular users So my thinking is, feedback should be only limited to site loading or process of campaign or some new features – rather then only complaining I think I also diverted from main topic – may be reason for conducting campaign is business too – but I am sure this is helping this forum by giving new regular users every year and new experts as Ayman said And DEEP, you are also here as a regular user after campaign so you should not asked this
And sorry DEEP but – this is one more useless discussion thread – and will go long as Umencho said because its on very sensitive topic Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to3 thankful Users |
7/8/2013 5:47 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Hello PISCEAN 2010, With reference to above subject only one reason i beleive & that is Motivation, Motivation & only Motivation That's it. |
Last edited by: Amit_86 at: 7/8/2013 6:16 PMNavang >> PISCEAN 2010(Thread Starter) I VANDE MATARAM..... |
|
This contribution was helpful to1 thankful Users |
7/10/2013 3:11 PM | |
Joined: 5/28/2013 Last visit: 2/1/2023 Posts: 112 Rating: (3) |
Its a nice way Siemens found to increase forum activity.. Increasing its activity, will also increase reliability in internet support because of the fast replies, and after that, Phone supports like Hotline doesen't get too much crowded
|
7/10/2013 7:09 PM | |
Posts: 9 Rating: (0) |
All about business. The easier it is to get technical help with a product, the more likely a product is to be used. It also motivates people like me to talk. In the past if I have a question, I search on here and I can normally find the answer. Te downside to that system is I am only here when I need something. By holding contest like this, I spend more time and so do many people like me, and you never know when we can help because of everything we have seen through the years.
|
7/10/2013 7:29 PM | |
Posts: 621 Rating: (10) |
in this forum i learnt more automation application tools.gain knowledge share knowledge..
|
Follow us on