6/23/2013 5:48 PM | |
Posts: 2964 Rating: (478)
|
Hello, May be current is drawing is more that why it is hunting? Have you checked the Smooth current actual value in the Service screen. Do you get any alarm in the screen ??? Check this DOCON WEB link regarding the alignment of the inceremental Encoder https://www.automation.siemens.com/doconweb/content.asp?item=13245&cd=sinumerik_simodrive_04_2010_e&scope=all Regards, Prakash |
6/24/2013 5:58 PM | |
Joined: 12/29/2011 Last visit: 8/9/2023 Posts: 39 Rating: (9) |
Hello Dhinakaran, The encoder and field windings most likely are out of alignment. You need a portable drilling machine, three 1000ohm resistors and a dual channel oscilloscope. Remove the motor mechanically from the machine. Leave the encoder connected to the drive reg card. Disconnect the three phase power connection to the servo motor at the LT Module. Mechanically connect a portable drill to the servo motor shaft to allow you to rotate it. Solder three 1000 ohm resistors in a star config. Connect the three free ends of the resistor to the u, v and w connections of the motor connector you disconnected from the lt module.. Connect an oscilloscope to the U phase connection and the star connection of the resistors. Connect an oscillsocope to the reference pulse from the encoder, please see the motor_connectors.pdf attachment. Rotate the motor shaft using the portable drilling machine and adjust the encoder position until you have a display which looks like the one on fig 110.1 of the waveform.pdf. All the Best Mr_Al. AttachmentMotor_Connectors.pdf (1429 Downloads) |
This contribution was helpful to5 thankful Users |
6/24/2013 6:00 PM | |
Joined: 12/29/2011 Last visit: 8/9/2023 Posts: 39 Rating: (9) |
More info.
AttachmentWaveforms.pdf (1483 Downloads) |
This contribution was helpful to4 thankful Users |
Follow us on