5/15/2012 2:20 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi The Status code of 08A0 satnds for: There is no free receive buffer available:No receive buffer space available for receiving data. Corrective action is :The P_RCV FB must be called more frequently. Please use the sample code which you can download fromhere. In this sample code inside FC11 there is a provision for sending two request of different data length from different area of a DB. Already programmed. And if required you can increase it further. Please see below
|
This contribution was helpful to1 thankful Users |
5/15/2012 8:46 PM | |
Posts: 559 Rating: (87) |
Dear Kaulquappe, I have also done the same thing & it was working fine. Dear Aevat, You can also try it. By the way you can also send telegrams individually to different slaves also in the same manner if you want to get data from more than 1 slave. |
This contribution was helpful to2 thankful Users |
6/12/2012 4:01 PM | |
Posts: 39 Rating: (4) |
hello sorry i have problem with opening the network/communication page, i have project that i want to send & recieve data with cp340 between servo drive (asda_a2 delta) with cpu 315-2dp, i run this assay to my project but i cannot: 1) find send & receive address 2) how can i send it or receive it? just by get address to them? this is my project attachment\ plz help me AttachmentZxx21_01.zip (98 Downloads) |
Follow us on