Industry Online Support
Technical Forum
7/5/2012 1:29 PM | |
Posts: 836 Rating: (100)
|
Check out this manualin chapther 1.5.2 and5.13. Here you find descriptions for this symbols. It sound like plausibility problems. |
10/10/2012 1:48 PM | |
Posts: 836 Rating: (100)
|
Hi, this is looking strange. Maybe its the best to create a Support Request. Before you make this check following question and attach the results to the Support Request. - Wich SW versions are you using? - PCS 7 V7.1: Start > Programs > SIMATIC > Information > Installed Software > Export - PCS 7 V8.0: Start > All Programs > Siemens Automation > SIMATIC > Information > Inst. Software > Export - Has the function a starting sequenser? - Has the function different control strategies? - Make a BCS Trace. To do this follow the insteuctions below: BCS Trace: - Open the Windows Explorer and go to path: "c:\program files\siemens\common\bin" - Start the application: "pcs7commontracecontrolx.exe" - In the dialog activate the option: "Enable Log" now the trace configuration editor opens - Choose the point: "BCS - Batch Control Server" > right click > "Modify Selection (recursive)" now the Trace Source Settings box openes - Select all options - Click OK and close the editor with STORE now the necessary settings are made After peroducing the effect the trace program writes the traces into the LOGS folder. You can find this folder under the same path like the trace program. Zip the LOGS folder and attach it to the SR. Don't forget to deactivate the trace program, becasue it needs a lot of performance. Good luck. |
Follow us on