9/11/2020 9:47 PM | |
Joined: 3/30/2016 Last visit: 4/6/2024 Posts: 11 Rating: (0) |
Hello to all, I made an ethernet connection between a LOGO (6ED1052-1MD08-0BA0) and S7-1200 CPU (6ES7214-1AG40-0XB0), using logo comfort 8.2 and tia portal V15. I use the guide I attached. The connection work correctly, but I have a problem in case of disconnection. The 2 devices are now connected by an ethernet switch. If i disconnect cable from LOGO to switch, when I reconnect it the connection is regurarly restabilished. But if I disconnect the cable from S7-1200 to switch, when I reconnect It the connection is not restabilished. Seem that LOGO restabilish connection only in case of cable disconnection. How can I be sure to automatically reconnect the devices after connection problems? I precise that I will use the 2 devices connected by a vpn, and I will need to use one or more switch between them. AttachmentEN_LOGO!-S7-1200_communication.pdf (186 Downloads) |
Follow us on