5/27/2016 6:45 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi Berg, The red wrench means that there is a input/output with a bad signal, which is device related. This is indicated by the "ST" part of a structure. When the "ST" parameter is 16#00, this means a bad signal, device related. Could you check all your connected inputs/outputs to check the actual value of "ST"? This could be the input:UserAna1, Rbk or any other signal which is defined as structure. Maybe, there is a signal which was created before, but deleted and the "ST" value is still 16#00. Normally, not connected inputs/outputs have the ST value: "16#FF". |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on