3/27/2018 1:22 PM | |
Joined: 1/27/2012 Last visit: 3/6/2024 Posts: 84 Rating: (1) |
Hello Experts, I am using a S7 400H system with all IO in redundant mode. I have programmed my logic between RED_IN and RED_OUT. I am using RED_IO52 library. I do know know where to call RED_DEPA. There is no clear information where and how to call this block. I have just called RED_DEPA in OB1 just before RED_IN block. Is this correct? Can you also check if I am using all redundancy related blocks correctly? My calling of redundancy blocks in different OBs: (Different DBs for each RED_DIAG) OB1: RED_DEPA, RED_IN, RED_OUT OB71: RED_INIT, RED_DIAG OB82: RED_DIAG OB83: RED_DIAG OB85: RED_DIAG OB86: RED_DIAG OB100: after end of my logic RED_INIT OB102: after end of my logic RED_INIT I am not using RED_STAT block. I use SFC51 for module status. like removed, error etc. I always get "Redundant I/O: Analog input channel error event ID 16#7982 also 16#7981" in diagnostic buffer. what is the reason? I am testing the panel without any signal connected to it. Diagnostic buffer is attached. AttachmentDiagnose.txt (105 Downloads) |
3/28/2018 9:36 AM | |
Joined: 11/14/2008 Last visit: 4/24/2024 Posts: 504 Rating: (22) |
Hi pradhan135 , For event id 16#7982 you can check this thread if you like : https://support.industry.siemens.com/tf/WW/en/posts/event-id-16-7982-redundant-i-o-analog-input-channel-error/172925?page=0&pageSize=10 Could you post the complete log here ? |
Follow us on