2/23/2018 8:57 AM | |
Joined: 4/6/2009 Last visit: 3/27/2024 Posts: 10 Rating: (0) |
Hello, I am using the Sitop Redundancy module for one of my projects and i am facing an issue for which i need a solution. I am using the redundancy module for 2 10A power supply and 2 5A power supply and i have this specific issue with the redundancy module connected to the 5A power supply. The LED on the redundancy module is glowing RED in color. What is the reason for the same? The Redundancy module connected to the 10A doesnot have any indication. What is the reason for the same? Also let me know me what is the significance of the LED and what should be done when RED LED glows and what should be done when GREEN LED glows? Photos attached. request help for this query. Regards R.Sureshkannan R.Sureshkannan ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/23/2018 2:38:32 PMNew subject after splitting |
|
2/23/2018 2:47 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, your connection is the same like the FAQ below? And look for the red led |
Follow us on