3/19/2009 10:24 PM | |
Posts: 2661 Rating: (279)
|
Hi Naishad, You should configure a WinCC client as a OPC XML DA server. If you want redundancy, you can configure a second WinCC client also as OPC server. The actual redundancy management should be implemented in the OPC client (MES system). See chapters 5 & 6 in the attached manual and see also the following link: Which OPC specification is contained in which version of WinCC? You need a connectivity pack license for each OPC server installation. Regards AttachmentOPC.pdf (73 Downloads) |
3/21/2009 1:09 PM | |
Posts: 61 Rating: (0) |
|
Follow us on