5/17/2011 7:12 PM | |
Posts: 11 Rating: (3) |
Hi Sarabjot, Are you using TIA Portal V11 for your PLC? If so, you can use the Data Logging feature to write a CSV file with the tag values you want to keep track of. I have posted an example program with a FB to set up and maintain a data log here. You may need to modify it for your application, but it would be a good starting point. Again, only really useful in this case if you are already using TIA Portal V11, but should be an easy solution if you are. Best Regards |
5/17/2011 7:33 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
How can WinCC exchange data with Microsoft Excel or Access? Best regards, Hristo Mihalev |
5/20/2011 10:03 AM | |
Joined: 2/6/2009 Last visit: 4/8/2024 Posts: 46 Rating: (23) |
Here is simple example of VBS script for writing tag values in csv file from WinCC. Best regards, VladD AttachmentWinCC_VBS_WriteTagInFile.zip (3620 Downloads) |
This contribution was helpful to5 thankful Users |
5/20/2011 2:08 PM | |
Joined: 10/3/2010 Last visit: 3/14/2024 Posts: 1552 Rating: (188) |
did you read the other replies above? Seems already an answer to your question in there |
B r g d s , |
|
5/30/2011 5:40 AM | |
Posts: 212 Rating: (12) |
Dear |
Follow us on