Industry Online Support
Technical Forum
9/30/2010 8:38 PM | |
Posts: 2 Rating: (0) |
Hello All, I am attempting to have 'Remote Control' of MP377 via a mobile device (BlackBerry or iPhone). I think that the issue lies with the 'Java' capability of the mobile device. System: MP377 12" Touch Panel, WinCC Flexible Advanced with Sm@rtService & Sm@rtAccess installed on panel. Connected to LAN with static IP. Details: I am able to Login to the HMI using a BlackBerry by entering my Name & Password. Three of the five links show up, missing 'Remote Control' and 'File Browser'. To get the 'Remote Control' - VNC Authentication screen I enter the specific address into the browser address 'http:// - IP Address - :RemoteControl.html' or 'http:// - IP Address:5800" I get an error. Question: Does anyone know if there is a way to get 'Remote Control' access to the MP377 using a BlackBerry or iPhone? I have attached a photo of the BlackBerry HMI Login Thank you, Blair |
2/18/2011 1:16 PM | |
Posts: 2 Rating: (0) |
I think also that the issue lies with the 'Java' capability of the mobile device. |
Follow us on