12/3/2010 5:29 PM | |
Posts: 3 Rating: (0) |
Hi all, I am going to built Remote control of control system remotly throuh the "Internet " I did the folowing: 1. Constructing ofa local LAN 2. Creating a project by WinCC flexile 2008 3. Setting of the Runtime Services in Device Setting " Sm@rtaccess or service: start up sm@rtserver " and " Sm@rtservice: HTML pages " 4. Running the project by WinCC flexible Runtime on the PC with IP address:192.168.1.2 5. At another PC with IP address: 192.168.1.3 I can control the PC HMI by Sm@rtClient The Proplem: When using Internet Explorer to monitor the system with the address:192.168.1.2 the integrated web pages does not appear and an error popup. How I can uses IE to do this? many thanks to all. |
12/9/2010 9:01 AM | |
Joined: 4/29/2010 Last visit: 3/19/2024 Posts: 1557 Rating: (161)
|
Hello, wich error pop up in this case? Do you have try other explorers like firefox for example? best regards. |
12/10/2010 8:31 PM | |
Posts: 3 Rating: (0) |
hello sir, the error is " this site is under construction " many thanks |
12/13/2010 3:21 PM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242)
|
Is it working on the same PC by entering http://localhost or http://192.168.1.2 ? |
Best regards, |
|
Follow us on