Industry Online Support
Technical Forum
2/6/2008 9:51 AM | |
Posts: 5822 Rating: (411)
|
Dear Roamingoat, well I have a good and a bad news for you. The good newsis that PG Routing to the PLC will work, as you have SIMATIC NET installed on the PC you want to use as Gateway. You will have to make sure that a configuration is loaded to it that allows you to do as you want. See this FAQ: Which requirements have to be fulfilled to perform a STEP 7 Routing via a PG/PC Station? The bad newsis that the HMI Devices will not work with this. In case of the HMI they require MPI or PROFIBUS to start from for PG Routing. Best regards J_Bell |
2/6/2008 10:57 AM | |
Posts: 5822 Rating: (411)
|
Hello, here you find the FAQ about this... it is the same situation for 2005 and 2007 How do you use WinCC flexible 2005 to transfer a project to an operator panel via S7 routing? Best regards J_Bell |
Last edited by: J_Bell at: 06.02.2008 10:57 |
|
Follow us on