6/4/2021 5:13 PM | |
Joined: 5/11/2020 Last visit: 1/2/2024 Posts: 8 Rating: (0) |
Hello, I have an ACS 800 ABB drive connected with s7-300 PLC Via Profibus RPBA-01 and I am trying to replace it with siemens G120 /CU250S.
the application is a wire rewind machine and it's working closed loop with encoder. also if you please could help with drive parameters to change and if there are any changes needs to be done in the plc program? the plc program is attached many thanks
AttachmentABB_repa.zip (139 Downloads) |
Follow us on