11/30/2012 5:10 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, The 200 series do not have a battery inside, there is however a battery module to retain the data for a longer period. Do you have such module at CPU? I don't think it has anything to do with your communication problem. Make sure you have the right cable and settings, try again with PLC in stop mode. Regards, Marcjan |
Problem solved? |
|
11/30/2012 8:10 PM | |
Joined: 12/22/2010 Last visit: 3/26/2024 Posts: 97 Rating: (0) |
Hello. My cpu is:CPU222 I can not connect by this plc and SF/DIAG &RUN leds are on I attached file My communication setting: Attachmentpic.pdf (157 Downloads) |
11/30/2012 8:25 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, Yes it's a 222, that's in the partnumber you mentioned Are there any modules connected or memorycard/baterry module placed at CPU? Remove all modules and start CPU again. Try all baudrate settings or select All baudrate (only works if pc adapter supports this) regards, Marcjan |
Problem solved? |
|
11/30/2012 8:48 PM | |
Joined: 12/22/2010 Last visit: 3/26/2024 Posts: 97 Rating: (0) |
hello, I remove all module and start cpu, sorry i can not connect by cpu( I tested all baudrate) |
12/1/2012 8:40 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, Well, if cable is correct and settings are o.k. only thing you can try is: Resetting the S7-200 to the factory default settings (WIPEOUT) For that you need a PC with Dos and the RS232 PPI adapter. Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
Follow us on