11/16/2021 2:08 PM | |
Posts: 1 Rating: (0) |
Hello, I need to replace a DC motor With a suitable ac motor as the equation torque=9554*P[kw]/rated speed the motor torque should be about 390 N.M at 1952 RPM I need to find a suitable ac motor, what is the correct motor power I should select? the old motor details is attached Many Thanks
Attachmentabb old dc motor.zip (693 Downloads) |
Follow us on