8/16/2015 6:43 AM | |
Posts: 45 Rating: (0) |
Hello Experts Team, I need Your help. Task is - To replace MP277 8" Touch HMI to TP 900" Touch HMI. HMI connected with Simotion. 1.During Device proxy creation after migration of HMI project from copy from step7 done into TIAv13 - Error comes during initialization that "PLC_Device Proxy fails" reason - unknown 2.Migrtation - D435-2DP , S120 and HMI MP277 to Only change TP900 ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/17/2015 2:21:55 PMNew subject after splitting |
|
8/17/2015 5:02 PM | |
Posts: 45 Rating: (0) |
|
Last edited by: Min_Moderator at: 8/18/2015 10:02:16 AMDelete quote |
|
8/17/2015 5:03 PM | |
Posts: 45 Rating: (0) |
|
Last edited by: Min_Moderator at: 8/18/2015 10:02:32 AMDelete quote |
|
8/17/2015 5:04 PM | |
Posts: 45 Rating: (0) |
|
Last edited by: Min_Moderator at: 8/18/2015 10:03:47 AMDelete quote |
|
8/17/2015 5:05 PM | |
Posts: 45 Rating: (0) |
|
Last edited by: Min_Moderator at: 8/18/2015 10:04:00 AMDelete quote |
|
8/17/2015 5:06 PM | |
Posts: 45 Rating: (0) |
|
Last edited by: Min_Moderator at: 8/18/2015 10:04:17 AMDelete quote |
|
8/17/2015 5:07 PM | |
Posts: 45 Rating: (0) |
|
Last edited by: Min_Moderator at: 8/18/2015 10:04:31 AMDelete quote |
|
8/17/2015 5:08 PM | |
Posts: 45 Rating: (0) |
|
Last edited by: Min_Moderator at: 8/18/2015 10:04:55 AMDelete quote |
|
8/17/2015 5:09 PM | |
Posts: 45 Rating: (0) |
|
Last edited by: Min_Moderator at: 8/18/2015 10:05:19 AMDelete quote |
|
8/17/2015 5:18 PM | |
Joined: 5/12/2006 Last visit: 3/28/2024 Posts: 22162 Rating: (2962)
|
Hello, ok you can't migrate the SIMOTION because this SIMOTION CPU and this Sinamcis are not supported in TIA. For SIMOTION you must use a SIMOTION D4x5-2 FW V4.3 or V4.4 and for the SINAMCIS S120 you must use CU320-2 V4.5 or V4.7. So you can only use the device Proxy in your case. How to use it is described here: https://support.industry.siemens.com/cs/ww/en/view/109476494 Regards |
8/17/2015 6:02 PM | |
Posts: 45 Rating: (0) |
Please can you check these two reference 1 and reference 2 file into attachment
AttachmentReference1.rar (260 Downloads) |
Last edited by: vaggmin at: 8/17/2015 6:04:03 PM |
|
8/17/2015 6:06 PM | |
Joined: 5/12/2006 Last visit: 3/28/2024 Posts: 22162 Rating: (2962)
|
i only see reference1 NOTE! Regards Christoph |
8/17/2015 6:08 PM | |
Posts: 45 Rating: (0) |
Sure, I will do that and send you the dropbox link. Thanks |
8/17/2015 6:12 PM | |
Posts: 45 Rating: (0) |
AttachmentReference - 2.rar (204 Downloads) |
8/18/2015 9:10 AM | |
Joined: 5/12/2006 Last visit: 3/28/2024 Posts: 22162 Rating: (2962)
|
Hello,
the D435 you use can't be updated to Version V4.4 . https://support.industry.siemens.com/cs/de/en/view/31045047
Regards Christoph |
Last edited by: ChristophD at: 8/18/2015 10:34:13 AM |
|
8/19/2015 9:53 AM | |
Posts: 45 Rating: (0) |
Hello, When i m doing fw update then the error come and still i am not able to update fw.Can you please give me the steps of fw update of "D435 Control Unit; Firmware V4.2 - PN V2.2 with SINAMICS S120 V2.6.2" 6AU1 435 -0AA00-0AA1 / V4.2
|
8/19/2015 10:24 AM | |
Joined: 5/12/2006 Last visit: 3/28/2024 Posts: 22162 Rating: (2962)
|
Hi,
ok if you use the device tool to create the update data you need the FWSP installed. The first link is the FW only, normaly extract the downloaded FW Zip File to the Root of a empty SIMOTION CF Card and put it in the CPU , the new FW is now loading at bootup from the CF Card. Note that you must also change the Version of the CPU in the project to V4.3 ! To do that open HWConfig and select the D435 V4.3 in thew HW Catalog and Drag&Drop it on the Rack of the D435 Station. If you don't update the CPU Version in the project then the device Tool can create the data for V4.3 and you can't work with the project if FW V4.3 isz on the CPU. I think is better you check if the Proxy init is working in you chase with Version of CPU V4.3. Regards Christoph |
Last edited by: ChristophD at: 8/19/2015 10:28:16 AM |
|
8/19/2015 11:01 AM | |
Posts: 45 Rating: (0) |
Sure i will try , that offline work of device proxy creation. |
8/19/2015 11:11 AM | |
Posts: 45 Rating: (0) |
|
8/19/2015 11:17 AM | |
Posts: 45 Rating: (0) |
|
8/19/2015 5:48 PM | |
Posts: 45 Rating: (0) |
I have one another problem that connection not making between HMI and Proxy Device. Device proxy data generation option also not coming into the software. |
8/19/2015 6:02 PM | |
Joined: 5/12/2006 Last visit: 3/28/2024 Posts: 22162 Rating: (2962)
|
Hello, have you read the description for the Device Proxy i have provided in early post? https://support.industry.siemens.com/cs/ww/en/view/109476494 please follow the steps in the document to solve this issue with the connection and the resynchronisation of the symbols! I hope you have resync an compile the winCC flexible part after the change of the CPU Version in Scout classic. Regards Christoph |
8/19/2015 6:19 PM | |
Posts: 45 Rating: (0) |
Sorry But i not understand the what you want to teach me with your statement - " I hope you have resync an compile the winCC flexible part after the change of the CPU Version in Scout classic."
|
8/20/2015 3:27 PM | |
Posts: 45 Rating: (0) |
|
5/23/2016 3:48 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4777 Rating: (123) |
New question published by vaggmin is split to a separate thread with the subject Communication in between ATLAS-COPCO Compressor and S7300 PLC. Best regards |
Follow us on