Industry Online Support
Technical Forum
9/29/2020 8:42 AM | |
Joined: 10/27/2015 Last visit: 2/8/2023 Posts: 2 Rating: (0) |
Dear Sir! I have a DC motor with specs V armature = 400 V I armature = 77 A V Field = 310 V / V Field = 240 V I Field = 1.75 A/ I Field = 1.4A Prated = 27.5 Kw speed = 2300 Rpm I wish to replace this old DC motor with AC motor Please suggest me suitable solutions to replace Motor unit. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/29/2020 11:28:39New subject after splitting |
|