6/24/2009 5:36 PM | |
Posts: 1 Rating: (0) |
Hello, When I generate Report system error, at 34% ofgeneration, it finish. I see just message in the window (left down) Generation not executed. But I don`t know why. I have CPU 319F-3 PN/DP. Thank you in advance. AttachmentRSE1.zip (141 Downloads) |
6/25/2009 2:57 AM | |
Joined: 10/7/2005 Last visit: 9/19/2024 Posts: 3021 Rating: (1054) |
Hello 2Pac please try the following: 1.) Do a compile of the whole project. To do so, right click on your Main project and select "PLC/Compile and downlaod objects" from the drop down menu. Tick the "Compile only" box, select all objects and start it. 2.) If 1.) does not help then do a "Save as" with "reorganisation" of your project and try again. 3.) If 2.) does not help, post our project here. I hope this helps Cheers fritz |
Cheers |
|
6/26/2009 2:04 PM | |
Posts: 510 Rating: (117) |
this FAQ may be helpful http://support.automation.siemens.com/WW/view/en/23576983 |
This contribution was helpful to1 thankful Users |
Follow us on