1/4/2015 8:31 PM | |
Joined: 10/31/2014 Last visit: 11/26/2022 Posts: 2 Rating: (0) |
Dear huggy, please take a while to read this msg. I have a rotary cutter (knife) application which cut the paper sheets to a given specific length without the mark indication accurately with a resolution of +/- 1mm. The total setup is supplied bya chinese supplier. Now i know only the drive is Ac servo drive (75kW) ith 50kw motor with encoder mounted on motor and extra encoder for measurement of length. Chinese supplied the whole setup with the embedded PC and software and lot of electronic cards for encoder and embedded hardware. I have the servo drive manual with parameter description. Now i want to remove all the embedded setup only want to use the same motor and the same servo drive but with Siemens S7-300 series PLC, FM354 module to program and a HMI for user interface. Please suggest the hardware required for the above setup with Siemens PLC and also please give a sample program for the above estimating the measuring wheel encoder is giving 5000 PPR. Please help me..... Thank you
------------ New subject after splitting from Incremental Encoder - I want to use it for reading leangth of a pipe. |
Last edited by: Min_Moderator at: 1/7/2015 10:20 AMSplitted |
|
1/7/2015 5:17 PM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating: (328)
|
I don't know the FM354, but I expect it can only be used for a rotary cutter, if the speed of the material to cut does not change (much). |
Last edited by: miami at: 1/7/2015 5:23 PM |
|
Follow us on