8/14/2016 9:09 PM | |
Posts: 7 Rating: (0) |
Hi, May I kindly ask some of your idea how to solve situation I have. What I need is to start motor at time=0 to the right direction, after 5 seconds it should stop and wait for 2 seconds, then it should run in left direction for 5 seconds. Everything I do produce in some moment that both outputs goes to 1 (which would lead to short circuit). Can it be done using ordinary ladder and existing timers or it have to be done using something other? Please find attached simplistic table of what I'm trying to do. Any ideas how to do that will be appreciated. Code should be run on LOGO! (never used until now). Kindly regards, Almir AttachmentTimers.pdf (158 Downloads) |
This contribution was helpful to1 thankful Users |
8/15/2016 6:15 AM | |
Joined: 12/18/2014 Last visit: 4/23/2024 Posts: 32871 Rating: (4064)
|
Here is a possible solution proposed in FBD and in LAD.
AttachmentReversing_contactor_circuit.zip (189 Downloads) |
This contribution was helpful to2 thankful Users |
8/15/2016 8:59 AM | |
Joined: 2/20/2014 Last visit: 4/23/2024 Posts: 395 Rating: (38) |
I would like to share a solution (which i guess is the same with what you would like to have). My circuit is based on the application example from Siemens (automatic shift register). Thank you
AttachmentReversing single phase motor with timers (different time on and off).zip (177 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on