11/25/2014 1:41 PM | |
Posts: 10 Rating: (0) |
Hi Owei, Can you help me with an example read program? Or if you can give me steps how to write a read program. Thanks.
|
11/26/2014 10:37 AM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71) |
Hi, sadly I don't have any example project for FB45 with TIA V11 and it's hard to explain via forum texting. Imean, if you could do an init_run, it's no magic to also do reads and writes. Just look at the FB45 manual: http://support.automation.siemens.com/WW/view/en/90063944 This manual was made for STEP 7 V5.5 but it works similar to STEP 7 V11. |
2/16/2015 5:24 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
3/10/2015 12:29 PM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71) |
Hi, which values did you use at "length" and "address MDS" in your MOBY CMD_d data block? |
3/10/2015 3:46 PM | |
Posts: 10 Rating: (0) |
all address are ok except MDS address 16#0. it required to change in command db (07CF for MDS D400)? |
3/10/2015 7:01 PM | |
Posts: 10 Rating: (0) |
there is no error on FB45 either RF180C Or Rf260R. Just want to confirm that the address MDS is the UID of MDS or Memory Length address? |
Follow us on