10/19/2018 7:17 PM | |
Posts: 1 Rating: (0) |
Hello, I have RLU 236 controller, and i want to control AC split unit via it, i am wondering if that is possible to control the speed of the evaporators fan (high, medium, low) depending on the temperature difference (between the setpoint and the temperature sensor), i.e. when the temperature difference is high, the high speed is on, and when the temperature difference decreases, the medium speed is on. not as in step, i dont want 2 or 3 speeds operate at the same time, it will burn the motor ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/22/2018 9:57:10 AMNew subject after splitting |
|