4/12/2015 9:11 AM | |
Posts: 30 Rating: (1) |
Dear experts, Is it necessary any HW configuration at step7 HW config?. if it necessary , please help me to find GSD file for 6ES7-972-0AA01-0XA0 . best regards saeed maghami.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 4/13/2015 4:27:16 PMNew subject after splitting |
|
4/12/2015 12:01 PM | |
Joined: 10/21/2013 Last visit: 9/19/2024 Posts: 417 Rating: (28) |
Hi, rs485 profibus repeater does not require any hardware configuration ..it can be directly installed .. |
2/17/2017 6:01 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684)
|
Hello xsmart; The repeater introduces a transmission delay in the network propagation, and the Profibus configurator should be made aware of the presence of multiple repeaters in the bus and the total length of the bus in order to recalculate the time delays introduced (Tbit value in network parameters). However you do not have to integrate the repeaters as separate modules in the network configuration. Hope this helps, Daniel Chartier Edit: If you would like to study the issue with more details, I can recommend this Technical Reference for Profibus-DP from Acromag; the last section (starting on page 36) is a discussion on bus timing and introduces the Tbit and Tsdr parameters that the Profibus configurator uses to synchronise the slave exchanges on the bus; https://www.acromag.com/sites/default/files/Acromag_Intro_ProfibusDP_698A.pdf |
Last edited by: dchartier at: 2/17/2017 6:03:12 PMLast edited by: dchartier at: 2/17/2017 11:20:15 PMLast edited by: dchartier at: 2/17/2017 11:32:52 PM |
|
This contribution was helpful to6 thankful Users |
Follow us on