10/20/2016 9:11 AM | |
Posts: 78 Rating: (0) |
SINUMERIK 810D CONTROL PCU20 MMC100.2 I have attached photos that may help Thanks for your time and help Regards Kevin Attachmentemail.docx (215 Downloads) |
10/21/2016 11:39 AM | |
Posts: 78 Rating: (0) |
Milling machine is running Ok We transfer programs from Laptop to milling machine using WININPC (windows XP) Programs are small so we run them from machine memory Milling machine has suddenly stopped communicating with laptop so we cannot load or backup programs When we try to send programs from laptop to milling machine nothing happens, we just get message Transmission in progress (see photo) When trying to send from milling machine to laptop the milling machine appears to be sending information but nothing goes to laptop I can send programs to the lathe (840D control) in the workshop which tends to indicate problem is with the milling machine not laptop/cable etc. All settings for sending programs are the same for mill and lathe except that mill would only work on RS 232 C Printer setting and lathe will only work on RS 232 C PG/PC setting I tried different Baud rates etc. but nothing worked I checked voltageof machine com port pins and they were the same for both lathe and mill (pins 2 and 4 had reading of approx. -8volts). Not sure if this means anything just thought I would see if milling machine had power going to com port This is the story so far RegardsKevin
Attachmentemail2.docx (148 Downloads) |
Last edited by: AutoGen_3276574 at: 10/21/2016 11:40:59 AMLast edited by: AutoGen_3276574 at: 10/21/2016 11:44:29 AM |
|
10/21/2016 12:06 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Check the selection of COM port, try first with COM 1 if it didn't work change to COM 2 & check. |
Follow us on