5/28/2014 8:48 AM | |
Posts: 95 Rating: (10) |
hi what is different between run and run-p? |
5/28/2014 8:51 AM | |
Posts: 10 Rating: (4) |
in Run-p mode you can download project in to the PLC but in Run mode only you can upload from PLC. |
5/28/2014 10:02 PM |
|
Posts: 784 Rating: (52) |
No problem |
5/29/2014 12:34 PM | |
Posts: 42 Rating: (1) |
so run is for up-loading program and run-p is for downloading, is that the only difference? |
5/29/2014 2:29 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, and for S7 400: S7-400: Operating Mode Switch at the new CPU 41x (as of FW Version 4.0) |
This contribution was helpful to2 thankful Users |
6/2/2014 5:34 PM | |
Posts: 72 Rating: (6) |
I really surprised to see this thread. For a just simple thing RUN & RUN-P there are total posts. Amazing..... |
This contribution was helpful to1 thankful Users |
Follow us on