1/31/2021 7:04 AM | |
Joined: 5/11/2017 Last visit: 2/4/2024 Posts: 59 Rating: (3) |
Please specify which SCADA you are using |
1/31/2021 11:48 AM | |
Joined: 7/3/2019 Last visit: 1/31/2021 Posts: 4 Rating: (0) |
It's runtime application on PC. |
1/31/2021 12:53 PM | |
Joined: 5/11/2017 Last visit: 2/4/2024 Posts: 59 Rating: (3) |
ExportImportUserAdministration DescriptionExports all users of the user administration of the currently active project to the given file or imports the users from the given file into the currently active project. Users, their passwords and rights are saved in the user administration. All users are overwritten when importing. The imported users are valid immediately. Use in the function listExportImportUserAdministration (File name, Direction) Use in user-defined functionsExportImportUserAdministration (File_name, Direction) Can be used if the configured device supports user-defined functions. For additional information, refer to "Device dependency". ParameterFile nameName of the file that contains the passwords or to which the passwords are written. Enter the file location and the file extension (*.txt), for example, "C:-TEMP-Passwords.txt". DirectionSpecifies whether passwords are exported or imported: 0 (hmiExport) = Export: Passwords are exported. 1 (hmiImport) = Import: Passwords are imported. I have attached test screenshots for configuration as well as runtime AttachmentScreenshots.pdf (290 Downloads) |
Last edited by: SahilU at: 01/31/2021 13:15:27 |
|
Follow us on