7/18/2019 7:37 AM | |
Joined: 4/28/2015 Last visit: 9/20/2022 Posts: 1278 Rating: (298) |
Hi, I can enforce the other writers as well. 1) using S210 or V90PN would be the better way nowadays (if you haven't bought the S110 so far), because it is easier to integrate to TIA Portal and the Technology objects 2) independent on the drive you use, I recommend to use telegram 105 in the drive and technology objects for positioning on the SIMATIC side 3) for safety I recommend to use a safe telegram (e.g. telegram 30) and using the ready to use library "LDrvSafe" in the safety program of the PLC to control all the necessary safety functions that are activated on the drive. The library contains blocks for each safety telegram and makes it very simple to control the functions of the telegram. Please check this out: https://support.industry.siemens.com/cs/ww/en/view/109485794 |
Best regards, |
|
7/23/2019 6:04 AM | |
Joined: 5/12/2006 Last visit: 9/23/2024 Posts: 22369 Rating: (3012)
|
helo, they are the same. regards christoph |
7/23/2019 8:40 AM | |
Joined: 5/12/2006 Last visit: 9/23/2024 Posts: 22369 Rating: (3012)
|
hello, check the S110 list manual https://support.industry.siemens.com/cs/ww/en/view/109476011 in Chapter 3.5 you find the informations there exist no example ! the only one is this: https://support.industry.siemens.com/cs/ww/en/view/58703073 Regards |
Follow us on