Industry Online Support
Technical Forum
10/26/2012 2:53 PM | |
Joined: 10/11/2006 Last visit: 4/26/2024 Posts: 5824 Rating: (789)
|
Hello,
You don´t have to parametrize the encoder (!)databecause safety uses the encoder informations from the drive - so you already inserted resolution (512)and fine resolution.(11). If you would use also a second encoder in addition (!) to your motor encoder then you can select and parametrize this in this screen.
Yes this is right - this information is most importan for SLS. See also in the function manual safety chapter 7.6.2.1
|
With best regards, |
|