12/17/2015 7:08 AM | |
Joined: 5/12/2006 Last visit: 5/13/2024 Posts: 22244 Rating: (2983)
|
Hello, which SW Versions do you use for Starter and Step7 ? Regards Christoph |
12/17/2015 8:12 AM | |
Joined: 5/12/2006 Last visit: 5/13/2024 Posts: 22244 Rating: (2983)
|
Hi, the prob is that in the STARTER Version V4.3 the SW DriceES Basic is needed for a correct integration of the Starter devices in Step7. Have you a driveES installation on the System? If no then uninstall Starter V4.3 , Install the Step7 SP4 and after that install the latest Starter V4.4. The latest Starter you can download here: https://support.industry.siemens.com/cs/ww/en/view/26233208 This message with Reason 211 means that there a some internal data not ok, this can happens if the wrong SW Combination is use for configuring the System.
Christoph |
Follow us on