6/2/2020 9:59 PM | |
Posts: 27 Rating: (1) |
Basically, I unplugged the drive cliq cable on the S210 drive (v5.2) to test its response, and I get an alarm (Tech alarm 108) which can not be acknowledged through the TIA portal Alarm Display, or through MC_RESET. Looking at the help-file for the Tech Alarm 108, it says to check the Status.Sensor for the "communication OK" parameter, and the "state" parameter. It also says that you can not enable the technology object again until encoder intialization is complete -- obviously, cycling power will reinitialize the encoder, but my main question is if there a way to do it in the software? Hopefully you can see the screenshots i've pasted below, uploading as attachment was not working today. [snip] ... AttachmentS210_Technology_alarms.zip (107 Downloads) |
Last edited by: CS Moderator at: 06/03/2020 11:30:58Picture as attachment |
|
Follow us on