7/25/2013 6:19 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hi Milos Petrovic The Process interrupt can be Triggered by Interrupt capable DI Modules like 6ES5 432-4UAxx or certain IP Modules. These modules are addressed in P Areas with address > 127 ( i.e. PW 128 onwards ) and not with 0 as commonly misunderstood. Additionally you need to do suitable settings in DX0 and Set the jumpers on the module. ( Pl see attachment ). There should be no DI module with address '0' installed. Can you post the exact configuration here ( CPU Type, Rack Type and Module Layout with addresses ), for better understanding ? Hope this helps Cheers Navnag AttachmentProcess_Interrupt_DI_432.pdf (188 Downloads) |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
Follow us on