7/4/2013 2:27 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
Hello, Sorry, the S5 series use TTY and therefor it's not possible to use the S7 adapter. You need an S5 card/adapter or if Eprom is fitted Eprom reader, Regards, Marcjan AttachmentconvS5.pdf (362 Downloads) |
Last edited by: Marcjan at: 7/4/2013 2:41 PMProblem solved? |
|
7/4/2013 2:30 PM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hello desmul24, You have to buy the Cablee for this, because on S7-300/400 CPU having MPI & DP port & on S5 there is a TTY port so both are different port So it will not work with Same cable on S5 PLC. Have a look on post S5 Cable Part number to be used for S5 155U cpu |
Ammy |
|
7/4/2013 2:44 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Hello, I am fully agree with friends here. Just want to add another solution for communicating S5 system with a USB adapters to suits modern laptops. You can select PG-USB from here:http://www.process-informatik.de/produkte/s5---interface&mt=1 Hope this helps.
|
Ayman Elotaify |
|
7/4/2013 3:26 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, I suggest you to buy adaptor instead of build one. Use the easy and safety way. Anyway, take a lookWhy does the online mode not work with the S5-PC converter TTY - RS 232? Best rgeards, Hristo Mihalev
|
Follow us on