11/15/2010 1:54 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
Hello, Look at Drive Note . The GSD flie DA020402.GSD you can find here. Just put "VLT5000" in search field. Best regards, Hristo Mihalev |
11/15/2010 2:19 PM | |
Posts: 19 Rating: (0) |
We've got this file but project had written in com-profibus 3.3 and for opening it necessary old file with extension *.200 |
11/15/2010 2:46 PM | |
Posts: 19 Rating: (0) |
We tried updated GSD list with this file but it didn't help. The same mistakes appears during opening existing project. |
11/16/2010 1:07 AM | |
Joined: 10/7/2005 Last visit: 9/20/2024 Posts: 3021 Rating: (1054)
|
Hello Vl@dimir COM Profibus V3.x allowed you to configure "DP Slaves" via GSD files as well as via .200 Typefiles. Your Danfoss drive was obviously configured with its.200 Typefile hencethe prolem you have right now. The way I see it, you have two options: 1.) Ask Danfoss for the .200Typefile for the driveand copy it into the TYPDAT5X directory of your COM Profibus directory. 2.) Reconfigurethe Danfoss Drive DP Slave by using its GSD file. I hope this helps |
Cheers |
|
11/16/2010 7:43 AM | |
Posts: 19 Rating: (0) |
We've written to Danfoss already. Will be waiting for reply. Thanks |
This contribution was helpful to1 thankful Users |
Follow us on