5/8/2012 8:53 AM | |
Posts: 3609 Rating: (29) |
Import of a Technical Question of the user ryan cordova
|
5/8/2012 12:24 PM | |
Joined: 7/18/2011 Last visit: 10/9/2023 Posts: 521 Rating: (90) |
Hi ryan cordova, Can you give us some more information about the FB's. What are their names? Maybe you can post printout of the code too ? Kind regards, BV |
5/12/2012 3:37 PM | |
Posts: 7 Rating: (0) |
Dear Sir; Their is no panel or any profibus or any other communication protocol is conected to the PLC, but their is MANUAL KEYPAD CONTROL PANEL going to the input byte 10 and E9.1 of the PLC, and this input are use in that blocks.. I just want to know what is the use of this blocks (FB210.FB221 and FB222) and if their is any posibility to convert this blocks in S7.. Please find the attached PDF file, and you will find how they are using this blocks.. Thank you.. Best Regards, Ryan
AttachmentS5 TO S7 BLOCK CANNOT BE CONVERTED.pdf (254 Downloads) |
5/13/2012 11:41 AM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, please send the code of these blocks. Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de
work faster withinnovative PLC-Tools |
5/20/2012 3:59 PM | |
Posts: 7 Rating: (0) |
Dear Sir; Please find the attach file. This is the code for FB210,FB221 and FB222 Thank You, Regards, Ryan Cordova
AttachmentFB 210,FB221,FB222 CODE.pdf (217 Downloads) |
5/20/2012 9:00 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, these blocks are "locked" from the creator. But i think the blocks are not from siemens. Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de
work faster withinnovative PLC-Tools |
Follow us on