1/31/2019 9:16 PM | |
Posts: 2 Rating: (0) |
Hello! To start, I dont have a lot of experience with S5. I have a PLC program file for SINUMERIK GA3 that I got from the CNC machime manufacturer. It was supposed to be the program for that exact machine. I can't open it with Step5 V7.2. When I try to open the file for transfer to PLC the software says "File error". I can't also open it with "S5 for Windows" or "PG2000". Is there any chance, that it may be a file from older version of step5 that's not compatible with these softwares? I have attached the file, so if anyone has a minute to check it, I'd be really grateful. Thank You in advance! //Rait AttachmentJBT537ST.zip (276 Downloads) |
3/6/2019 4:07 PM | |
Joined: 7/15/2008 Last visit: 1/23/2024 Posts: 382 Rating: (44) |
Hello, I tried to open for file on an old PG710, and it also gave me the File Error. I am assuming you got an upload of the PLC that is corrupted. Can you ask the CNC OEM to send you a propper backup. They should have everything you need. For your reverence I included a PLC Backup of an old 820 CNC, so you can see how it should look like. Regards / m.f.g AttachmentOP120TST.zip (260 Downloads) |
Follow us on