11/2/2015 4:30 PM | |
Posts: 439 Rating: (108) |
Hello drv, Those are Diagnostics indication LED as you can see here. Go into the properties of the signal board and activate the boxes:
Those are suppose to be check by default. Then, you just have to test it by going under or over voltage. Best regards, Hugo |
11/3/2015 6:09 AM | |
Joined: 7/14/2015 Last visit: 5/5/2023 Posts: 2 Rating: (0) |
Dear Sir, Thank you very much for your Support. I am agree with you that this LED for Diagnostics indication. But I want to know that if I take first LED : then what is indicate? Second LED : Third LED : etc.. In that way i had to give information to trainee Engineer. So, Sir please provide me this type of information. Also find below attached photo. In that photo i can only change Short circuit diagnostics if it is use as voltage. I Can't change overflow / under flow diagnostics. |
Last edited by: drv at: 11/3/2015 6:10:59 AMLast edited by: drv at: 11/3/2015 6:11:54 AM |
|
Follow us on