4/2/2014 11:28 AM | |
Posts: 4 Rating: (3) |
Hello , I am trying to accomplish Profinet communication between S7-1214C and two S110 servo drive for several days: - I added S110 GSD file in the TIA portal - I set IP of each device - hardware connection works fine. - I added a telegram in TIA portal with many difficulties - I set drives by STARTER: model, power module type, IPs, same telegram, some base settings - I added DPRD_DAT and DPWR_DAT blocks in OB1 and connected them to the hardware constants by drag-and-drop ...... But there is no communication between the devices. Starter displays alarms #8511 COMM BOARD: Receive configuration data invalid & #8526 PROFINET: No cyclic connection; DPRD_DAT shows alarm 16#80A0 in RET_VAL output DPWR_DAT shows alarm 16#80A1 in RET_VAL output I'm tired of looking at posts in the forum. I'm tired of looking at how to make communication between G120 and S7- 300 in the old version of STEP7. In the attached archive you will find pictures of the settings . Which settings are not made properly? Has anyone managed to connect the S7- 1200 PLC with two (or one) servo drives by Profinet or that is impossible? Also I tried to connect RECORD output of DPRD_DAT to structure, but it gives me an error, so I'veconnectit to an array. Why it is explained in a document how to use structures for that, I do not know?
AttachmentProfinet problem.zip (725 Downloads) |
This contribution was helpful to1 thankful Users |
1/14/2016 6:38 AM | |
Posts: 1 Rating: (0) |
Dear all,
Kindly give any sample program for s7 1214 V13 S7-1200 and S110 Profinet communication I am going to take a project of postion control.
Regards, G.Venkat LGB-MBD-India automation Engineer |
1/14/2016 7:13 AM | |
Joined: 5/12/2006 Last visit: 9/24/2024 Posts: 22371 Rating: (3012)
|
Hello, 1.) Don't post a question not more then one please! Have a look in this example: https://support.industry.siemens.com/cs/ww/en/view/98961635 The basicals are the same for S120 and S110. Regards Christoph |
4/8/2016 8:52 AM | |
Joined: 9/30/2015 Last visit: 9/7/2022 Posts: 23 Rating: (0) |
how |
4/8/2016 9:11 AM | |
Joined: 5/12/2006 Last visit: 9/24/2024 Posts: 22371 Rating: (3012)
|
what you mean? |
Follow us on