Industry Online Support
Technical Forum
10/3/2011 3:56 PM | |
Posts: 1 Rating: (0) |
Hallo, I'm new user here on the forum and I'm searching for working ( if exist ) solution, how measure temperature with temperature sensor SMT-160 connected to PLC S7-1200 ( CPU 1212C ). Signal from SMT-160 is PWM - so I need to now how long is "on" signal an how long is "off" signal to calculate measured temperature. Is there somebody with experience with this sensor ? I checked a lot of posts, but I can't find information about working solution. Thanks for help Alda for more information about SMT-160 please check attachment Attachmentsmt_smt160.pdf (143 Downloads) |
5/23/2016 10:57 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by AutoGen_948162 is split to a separate thread with the subject Can i connect tamperature sensor without rtd module?. Best regards |