4/28/2017 9:49 AM | |
Joined: 12/29/2008 Last visit: 9/17/2024 Posts: 24 Rating: (3) |
Very simple solution, it is to use MODBUS TCP on S71200 and gateway Fieldserver MODBUS BACNET TCP You can find it here: Gateway BACNET-MODBUS Very simple to configure and to use. |
This contribution was helpful to1 thankful Users |
8/2/2017 8:35 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by andres.sandoval.1984 is split to a separate thread with the subject Is it possible to get information of Bacnet devices from two PLC through of Gateway UGW Micro Profinet? . Best regards |