1/16/2013 9:36 PM | |
Posts: 5 Rating: (0) |
I have still no luck in getting a connection. I found a instruction of KEYENCE barcode readers. But i'm not sure it will be the same for the barcode reader I use. ( DataLogic D100) But anyway I build the hole circuit and so far so good. No Errors But it seems that there is no connectieon beween the reader and the PLC. The port settings are set equal. Do the indicator lights on the CM1214 light up when they get a signal from the read barcode? They are dead in my case. I'm a bit lost... I tried different port settings but no reaction on the module or in the watch tabe. Within the attachment you will find the instruction. I have build the circuit untill page 21 I hope that someone can push me in to the right direction! AttachmentInstructieBLSR_S7-1200_RS232C_0_E.pdf (2178 Downloads) |
3/25/2013 8:37 AM | |
Posts: 1 Rating: (0) |
Are you trying to find barcode solution? I intended to create barcode in C# and read barcode in C# last month and I found good solution there. Hope this is a helpful clue. |
6/13/2013 4:51 AM | |
Posts: 2 Rating: (0) |
If you wanna save these complicated steps and find a easy way, you can google barcode scanner and you will find many useful tools, or google how to read barcode in c# to get instructive articles. Good luck:) I think some imaging sdk programmes can enable to quickly scan barcodes. i have use imaging sdkr which can original layouts hyperlinks, Images and tables retained in word ,text, image, Epub, html.but i forgot download the wedsite ,go to google. By the way , pay attention to your system platform, select the suitable one . I use a barcode scanner driver found on the internet . Install it and it becomes a selectable option.Then you can scan barcodes in many formats in any program at all, including Adobe Acrobat . Just open the sdk, select barcode, and choice a form you want, then you can scan barcode in c#, vb, sdp ,etc ,the task will be finished in several seconds. if you haven't found a good choice , you can have a try. best wishes. |
7/26/2013 5:26 AM | |
Posts: 1 Rating: (0) |
Thanks for sharing this. It is amazing!!! I find my barcode solution there. |
12/18/2013 10:17 AM | |
Posts: 2 Rating: (0) |
Howdy, thanks for sharing but I'd like to know how many symbologies does this barcode reader supports? I've checked the page and I didn't see what types it supports. |
9/28/2014 5:05 AM | |
Posts: 2 Rating: (0) |
What kind of program do you refer to, for .NET, Java...? |
Follow us on