8/26/2020 5:00 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello Analytical Apprentice; Just to add an example of the I/O capabilities of a S7-1200, here is a screenshot taken from the S7-1215C Technical Data. https://support.industry.siemens.com/cs/pd/142915?pdti=td&dl=en&lc=en-WW The process image can deal with 8196 inputs and 8196 outputs, but the main CPU can connect only to 8 I/O modules only; the rest can come either through Profinet IO or Profibus distributed I/O stations. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 08/26/2020 17:03:29 |
|
This contribution was helpful to2 thankful Users |
Follow us on