6/16/2018 6:42 AM | |
Posts: 1283 Rating: (105) |
i am just using the GET directly in OB. First thing is that i am not sure the S7 communication is successful. I had attached my setting i had done so far. please correct me if i miss something.\ Jay AttachmentGET.doc (102 Downloads) |
6/16/2018 7:10 AM | |
Joined: 12/18/2014 Last visit: 4/24/2024 Posts: 32871 Rating: (4064) |
As I already wrote: AttachmentGET.zip (118 Downloads) |
6/16/2018 8:11 AM | |
Joined: 12/18/2014 Last visit: 4/24/2024 Posts: 32871 Rating: (4064) |
Did you remove the check mark "Optimized block access" at DB1? |
6/16/2018 8:48 AM | |
Joined: 12/18/2014 Last visit: 4/24/2024 Posts: 32871 Rating: (4064) |
No. I use V14 SP1. |
6/16/2018 9:04 AM | |
Posts: 1283 Rating: (105) |
this is my LoGO program. nothing in it. just one sensor. You can create a project with CPU 1212C DC DC DC , ip address 192.168.255.3. Thank you so much for all the response. You are the best. I am just trying the same to be you to help as much as I can. Jay AttachmentDRY COOLER.zip (94 Downloads) |
6/16/2018 10:00 AM | |
Posts: 2826 Rating: (684) |
My apologies for stepping into this conversation uninvited and late. I could get that method to work correctly between CPU1212C and LOGO! ixo65 - if you would be willing to share the project files you used, I would be most happy to have a look at them. There is one detail that is missing from the PDF. The PUT-GET needs to be given permission to take place; even if there is no GET-PUT instructions mentioned in the PDF. I will be willing to share what I know - but maybe consider opening a new topic(?). Regards. |
Follow us on