3/10/2011 12:11 PM | |
Posts: 1 Rating: (0) |
THANKS!!!!!!!!!!!!!!!!!!!!! I test it and run prefect. I love you man. |
3/10/2011 1:30 PM | |
Posts: 5 Rating: (1) |
Contact me via PM and i will give youa link to get the Modbus TCP Client and/or Server for the 1200. |
6/16/2011 11:33 PM | |
Joined: 8/18/2010 Last visit: 3/18/2023 Posts: 42 Rating: (9) |
It does not seem that the files are still available when you follow the link. Does anyone have another link? I am also looking for both the Client and server Modbus TCP for the S7-1200. I looked at the one by Siemens (CE-x22) but it was only designed to communicate via function code 3, 40001 registers. I need to poll 10001 and 30001 registers as well. Any help would be appreciated. |
6/17/2011 3:07 PM | |
Joined: 7/7/2010 Last visit: 4/25/2024 Posts: 14629 Rating: (2349) |
Do you want to read from the PLC or write to the PLC from another device? |
science guy |
|
6/18/2011 2:06 PM | |
Joined: 1/17/2007 Last visit: 4/26/2024 Posts: 1542 Rating: (531) |
An alternate approach could be to use a modbus RTU to modbus TCP convertor. I have used the XPress DR-IAP in the past and it has worked well. It just converts modbus RTU protocol to modbus TCP protocol, so it can be client or server depending if you use master or slave RTU. |
Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots. |
|
7/15/2011 2:24 PM | |
Joined: 5/28/2008 Last visit: 4/26/2024 Posts: 1343 Rating: (141)
|
Here you'll find updated code for v11: http://support.automation.siemens.com/WW/view/en/40614428 regards |
Follow us on